Cancel
Showing results for 
Search instead for 
Did you mean: 

Flattening and Forming

Phenom
Phenom

In the past the flattening and forming utility has moved around inside the different Mach bundles, been a seperate add-on, etc.

In NX 11, which licenses provide access to the Flattening and Forming tools? I'm not talking about sheet metal flat pattern. This is the tool to flatten surfaces and points.

9 REPLIES

Re: Flattening and Forming

Phenom
Phenom

I got it in Mach 3 with PDW.

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Flattening and Forming

Phenom
Phenom
Sure hope it's in a lower level than that!
Thanks for the information.
I have an older functionality spreadsheet but it doesn't appear to include the Flattening and forming as a "module". So I can't tell where it's located. There is a line for Advance Sheet metal Design and it does show that it is in Progressive Die Design. But this is a common type function when you have to work with imported solids or sheet metal parts that don't have a flat surface on them.

Re: Flattening and Forming

Phenom
Phenom

This is what NX is calling in the Log file. UG_MODELING_FF_FLATTENING_FORMING

Re: Flattening and Forming

Phenom
Phenom

How many parts have you got to flatten?

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Flattening and Forming

Phenom
Phenom

THe request is coming from my parent company (Aero/Defense/Auto). If you are offering to flatten them I appreciate the offer. Due to IP and NDAs I can't share. They will need to decide if there is enough business reason to upgrade a seat or purchase the floating Adv Sheet Metal module.

Re: Flattening and Forming

Gears Phenom Gears Phenom
Gears Phenom

I have it in our "NX Mach 3 Prod Design" bundle. 

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Flattening and Forming

Phenom
Phenom

Hmm. Maybe they pushed it down into the Standard Mach 3. That would be good!

Re: Flattening and Forming

Gears Phenom Gears Phenom
Gears Phenom

One of our guys took the sheetmetal class right around the time NX11 came out, and I recall him saying the 'new' forming and Flattening would be included.

 

(I say 'new', because it reminds me a lot of the old flat pattern tool.)

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Flattening and Forming

Phenom
Phenom

I'm fairly certain it is not in a Mach 2 license. That is what the user is currently using and getting licensing error message.