03-13-2017 05:24 PM
Hello all,
SO long story short, there's a random glitch that occurs when I subctract two solids from each other...
And then, THIS DONUT appears!
Has anyone else had something similar? We can not get rid of it.
If anyone has experienced similar, we'd like to hear.
Thanks,
Ray
Solved! Go to Solution.
03-14-2017 05:36 AM
Hi,
This is probably a face that is not trimmed correctly. Without the actual part there is not much we can say about it.
Regards, **bleep**
03-14-2017 09:13 AM
Hi,
I did not model the floating donut. It just appeared out of no where.
Is this common? This has happened on two parts now.
Regards,
Ray
03-14-2017 09:34 AM
So you are subtracting solid B from solid A
I'm suspecting solid B has a "hole" in it.
If you do a "modeling" section of solid B (before the subtract), is the cross section "solid" or is there a "hole"?
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled
03-14-2017 11:00 AM
Hope this helps visualize...
The green part is B
Cross sectioned, it is solid.
This yellow block is A
When Cross sectioned, it is also solid.
Now, Subtracting B from A looks like...
Final product is this... with a floating donut shape... where does this come from?!
03-14-2017 11:39 AM - edited 03-14-2017 11:43 AM
I'm guessing that one of the blends is ignoring its trim boundaries after the subtract command.
I've seen something similar when a blend face ran amok. I ran the "examine geometry" command and found that one of the bodies had some geometry errors that needed to be fixed. After the corrections, the part behaved in the expected manner.
03-14-2017 11:58 AM
Were both of these parts created from scratch in NX? If they weren't you could try using the Optimize Face command to clean up the geometry and as @cowski1 suggests, use Examine Geometry to locate any potential issues. I've seen similar issues that were sent to the Parasolid development team to review, so if you're not able to resolve the condition please consider opening a new IR with GTAC.
You tagged this NX10, but are you using the latest version; NX10.0.3? Do you have NX11 available to test the same boolean? I'd be curious to know if it's something that occurs in newer versions.
Regards, Ben
03-14-2017 01:10 PM
We use both NX8 and 10 at the moment. We have an available upgrade to 11... In this long process of transitioning over.
Our license server currently does not have 11 available.
I will try Optimize Face and Examine Geometry.
03-14-2017 01:26 PM
Ben,
I can not believe this worked.
The DONUT IS GONE!
Thanks!
03-14-2017 01:32 PM