Cancel
Showing results for 
Search instead for 
Did you mean: 

Getting error while opening PTS

Pioneer
Pioneer

Hi everyone.I am new to NX and currently using NX9.I am trying to using PTS but getting error while opening PTS.

Have a look at error message.Please give some inputs to resolve this error.

Thank you.

5 REPLIES 5

Re: Getting error while opening PTS

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

did you set the UGII_JAVA_HOME environment variable?

From NX8.5 java path location isn't default set in NX.

 

try to set the UGII_JAVA_HOME  in the system environment settings (point it to the location of the JAVA install)

after that try to start PTS again.


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Getting error while opening PTS

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Also, make sure you're pointing UGII_JAVA_HOME to a 64-bit version of Java.

 

Another trick is to open the NX Command Prompt and enter "pts".  You can manually define the path to UGII_JAVA_HOME and you'll get more system feedback in the command window than you would if you attempt to launch PTS from the Windows Start menu.

 

Even better - upgrade to NX 11 (or newer).  The PTS Author application is embedded in NX now.

 

Regards, Ben

Re: Getting error while opening PTS

Pioneer
Pioneer

thanks ruud.I will try to implement your solution.

Re: Getting error while opening PTS

Pioneer
Pioneer
thank you BenBroad.

Re: Getting error while opening PTS

Pioneer
Pioneer

i installed java 7u80 and restarted pc.And run the PTS.It worked.