Cancel
Showing results for 
Search instead for 
Did you mean: 

Given matrix is not from the required part

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi,

 

wired thing. since a few days this situation appears while loading a released part in teamcenter. we use NX9.03 MP15 and Teamcenter 10. and then it comes up while loading in with "Given matrix is not from the required part"

 

If i have an assembly opend and i load another on this error occurs. If i load the fail part standalone the same error occurs. if i load structure only it works. But only if i start to laod parts. Same error

 

Any ideas where this error comes from? How can i fix it?

 

Could not find anything with google, here or @gtac about this

1 REPLY 1

Re: Given matrix is not from the required part

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

problem solved by reinstalling and updating again to mp15.