Cancel
Showing results for 
Search instead for 
Did you mean: 

Going from the model to the drawing

Honored Contributor
Honored Contributor

Using NX with Teamcenter...

 

Users ask about this one a lot.  If you have a model open, and then want to open the drawing, is there a quick and easy way to open it?  Other than going to Teamcenter and searching or browsing for it?  Ideally they would like to select the model (on screen or in the assy navigator), and right click open drawing (or get a list of drawings if there is more than one).

 

I'm not aware of any way, but figured I'd ask, since my TC experience is limited.

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10
1 REPLY 1

Re: Going from the model to the drawing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Here is a journal that may help.

 

p.s. I am not the author of this code, but it looks like it would be helpful.