Cancel
Showing results for 
Search instead for 
Did you mean: 

Graphical glitches when rendering after adding more parts to assembly

Experimenter
Experimenter

Since adding more parts to an assembly, I have the graphical glitch, where edges appear weird and things are on top of each  seen in the image below on certain frames when rendering animation frames (through View--Visualization--Create animation), making the resulting animation unusable.

 

I've Googled around like crazy and tried different changes including changing the model thickness and messing around with visualization settings, and even tried the same animation rendering on four different computers, but always getting the same issues.

 

If I pause the rendering and rotate the view, it goes back to normal. Is there any way to force NX to do the same thing before rendering each frame?

example.pngGlitch