Cancel
Showing results for 
Search instead for 
Did you mean: 

Graphics issue

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hello all,
One of my client is using NX 10 AND NX11 ..and he's using Nvidia quadro k2200 graphics...Nx 10 is working fine without any issues but in nx11 he's facing graphics issue like if he draws a circle if he zooms back it would appear like small piece of points and when he zooms in it would be normal..only in nx 11...
He is using win8..with 16gb ram
2 REPLIES 2

Re: Graphics issue

Siemens Phenom Siemens Phenom
Siemens Phenom
Since it's a graphics issue. Have you tried to update the graphics driver? Might just solve the issue. From the screenshot you provided could not see the driver version for the graphics card.

Kind regards,

Dennis
Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: Graphics issue

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Thanks @DennisdeBrouwer..
It worked 😊