Cancel
Showing results for 
Search instead for 
Did you mean: 

Helical groove in NX9

Valued Contributor
Valued Contributor

Hi,

I have an hollow cylinder, OD 150 and ID 100. I have created an helical groove of 2x2 on outer periphery. There is an sharp corner developed at the start and end of helical groove. I would like to apply a small blend on that sharp corner. Let me know which option will help to create blend.

 

Thanks

Yunus

5 REPLIES

Re: Helical groove in NX9

Siemens Phenom Siemens Phenom
Siemens Phenom
Without seeing a picture of your part, have you tried Edge Blend?

Re: Helical groove in NX9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Or face blend?

Re: Helical groove in NX9

Valued Contributor
Valued Contributor

Hi,

Please find the attached part file "Helical Groove.prt" and "Blend.png". I would like to apply 1.6 mm radius at sharp corner produced by helical groove at start and end of the groove.

Hoping you will do the needful.

 

Thanks,

Yunus

Re: Helical groove in NX9

Phenom
Phenom

Assuming you want sharp corners in the groove, enable "Preserve Shape" in the swept feature.

 

Extend the helix by +- 1 turn so it breaks out of the end faces

 

edge blend works fine with clean geometry

 

part attached

Re: Helical groove in NX9

Valued Contributor
Valued Contributor

Hi,

Thanks for sharing the updated model. I will go through and let you know if anything is required.

 

Thanks,

Yunus