Cancel
Showing results for 
Search instead for 
Did you mean: 

Help Unbend/Rebend Sheet metal enviroment.

Builder
Builder

Hello,

 

I'm using NX 9.0 but never I'm using the Sheet metal enviroment. I need some help:

 

I have a piece done in Sheet metal enviroment and at the end I did the Unbend operation. Then I see the part completely unbend.  But also I need the isometric figure. How I can see both, unbend figure and Isometric figure.  I need both of them in Drafting enviroment.

 

Apreciate some help

 

Thanks

 

Jose C.

2 REPLIES 2

Re: Help Unbend/Rebend Sheet metal enviroment.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @JCP,

 

You say you have used the unbend feature. This is normally used to temporarily unbend one flange, make a change on the model, and bend it back again.

 

If you want to have a flat-pattern, you should use the Flat-pattern option. Smiley Happy

 

If you now look under Model Views in your part navigator, you'll see probably the trimetric is work view, double click the Flatt-pattern to show the flatt-pattern, and do the opposite to work again on the model.

Ashampoo_Snap_2016.11.11_15h14m36s_004_.png

When you are in drafting, you can select which view you want to place on your drawing... the flat pattern should now be one of them.

 

Kind regards,

 

Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: Help Unbend/Rebend Sheet metal enviroment.

Builder
Builder

Thanks Dennis! 

Problem solved!

 

Good day

 

Jose C