Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Help with creating a nest between two bodies.

Experimenter
Experimenter

Hello Everyone. I am a new NX user. Most experience is with the CAM side. Looking for a direction to go in for this problem. We are manufacturing small medical components. This requires a nesting fixture. In the pics I have projected the profile of the component and extruded the profile up. The nest is the extracted faces of the component. How can I join these two so it is a solid? I have tried Extrude/Subtract.I know how to create a ribbon surface between the two I can machine to but it is hollow inside and would prefer a solid. Any help is appreciated.

4 REPLIES 4

Re: Help with creating a nest between two bodies.

Valued Contributor
Valued Contributor

you want to close the extruded body with the fancy curvy face on top?

Re: Help with creating a nest between two bodies.

Experimenter
Experimenter

Yes. Thanks. I may have come up with a solution. After projecting the profile. I extracted the faces. Then used the thicken command. After extruding past the shell I used the emboss command to create an extruded post with a nest on top of it. I know there is probably a better way. I appreciate the help. Now I'm trying to put draft aroung the nest to the Blue colored surface.

Re: Help with creating a nest between two bodies.

Siemens Phenom Siemens Phenom
Siemens Phenom

@ISUZU_NPR_GUY,

Depending on the actual geometry, you may be able to simply use 'Until Next' for the limit of your extrude. That way you won't need the emboss feature.

until next.png

Regards,
Abe

Re: Help with creating a nest between two bodies.

Legend
Legend

Hi @ISUZU_NPR_GUY

 

I very similar with my example part of 'Draft Body' command.

 

I am not sure, the 'Draft Body' is successful for your case too.

 

Please try to use 'Draft Body' command [insert > Detail Feature > Draft Body]

- Type : Faces to Draft

- Parting Object : Top face of Base Body (Blue color of your image.)

- Draw Direction : (same with Draw Direction of draft)

- Faces to draft : All faces of target body

- Draft Angle : angle value.

 

Anyway Good luck.

 

 Sunkap Ahn, Senior Support Engineer


logo