Cancel
Showing results for 
Search instead for 
Did you mean: 

Hidden one part when start work part Assembly

Experimenter
Experimenter

Dear friends,

My part is vissible only when work part. And invissible after moving to assy structure.

Why this happened. I can not solve it.

Thank you in advance

3 REPLIES 3

Re: Hidden one part when start work part Assembly

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Denis Dubas

 

You have to check the setting of your reference sets. With the assembly open right click on the part (your previous work part added to the assembly), select replace Reference Set and chose correct referense set listed (selecting Entire Part will show you everything in the component)

 

Best Regards

Fred

 

2018_07_25_12_32_31_NX_12_Modeling.png

 

 

Re: Hidden one part when start work part Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Other options:

layer settings

- right-click on compnent in Assembly Navigator -> Properties - what layer setting was used?

- depending on above, what layers are the objects on in the component - are those layers visible in the assembly?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Hidden one part when start work part Assembly

Experimenter
Experimenter

Thanks. It's working.