Cancel
Showing results for 
Search instead for 
Did you mean: 

Hiding NX-->file-->Tab menu

Builder
Builder

Hello All

 

How i want to display "Model" and Drawing Tabs only. how can i hide all others

 


NX.PNG

 

Thanks

5 REPLIES 5

Re: Hiding NX-->file-->Tab menu

Siemens Phenom Siemens Phenom
Siemens Phenom

This is controlled through the PAX files. The following link is a good place to start.

 

PAX Files

 

Scott

Re: Hiding NX-->file-->Tab menu

Builder
Builder
Thanks Scott

These pac file control each tab, is there any single config containing the display of these tabs, where i can selectively hide the tabs?

Re: Hiding NX-->file-->Tab menu

Honored Contributor
Honored Contributor

Not that I have seen.  If a pax file exits in the folder, the tab will be shown, so it's an all or nothing deal, not user selectable.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Hiding NX-->file-->Tab menu

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @nesthome!

For each application/tab, there are separate PAX files.

You have to edit the individual PAX file. I checked it for Modeling and Drawing tab, Just add "<! --" in PAX file (Comment out for XML) as shown in the image. Edit the respective PAX files, Save and restart NX, you will not see those tabs.

pax.png

 

Re: Hiding NX-->file-->Tab menu

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Set the variable UGII_TEMPLATE_DIR to a folder.
Copy the PAX file and the templates file into that folder.
When starting NX it will only show the things that are in that folder.

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions