Cancel
Showing results for 
Search instead for 
Did you mean: 

High Quality Image Error NX 11

Experimenter
Experimenter

Hello Everyone,

 

There seems to be a change in High Quality Image exporting in NX 11. A command I had no problem with in NX10 doesn't work in NX11.

It says " This command is available when the NX_RTS_IRAY environment variable is set to 0, which turns off the new Iray+ renderer."

Anybody know what that means?

 

hgi.png

 

2 REPLIES

Re: High Quality Image Error NX 11

Siemens Phenom Siemens Phenom
Siemens Phenom

With the new Ray Traced Studio rendering the static image generation is now part of that workflow.

 

2017-03-01_6-54-42.pngStatic Image Generation

Try this out with NX 11. There videos posted in the Knowledge Base to show how the new rendering works and what the advantages of this are over the old methods.

 

Scott

 

Re: High Quality Image Error NX 11

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Elif,

In NX 10, command 'High Quality Image' is available under Menu > View > Visualization.

From NX 11, this command is not available by default. As in command finder it describes, set the environment variable 'NX_RTS_IRAY' with value '0' on your system, restart NX 11 then you will be able to access this command.

 

Regards,
Ganesh