Cancel
Showing results for 
Search instead for 
Did you mean: 

Hole Callout support for multiple hole not in a Pattern

Valued Contributor
Valued Contributor

Can the number of holes be shown on a hole Callout when they have been created in one holes command using multiple points, and not the pattern feature.

 

Sometimes we have a series of holes in an irregular pattern.

Martyn, Principal CAE Engineer, Renishaw PLC
NX12 Tc12
2 REPLIES 2

Re: Hole Callout support for multiple hole not in a Pattern

Siemens Phenom Siemens Phenom
Siemens Phenom

By using the 'General' Layout scheme you can create Pattern Features which can be irregular yet still recognized as a true pattern.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA
Highlighted

Re: Hole Callout support for multiple hole not in a Pattern

Valued Contributor
Valued Contributor

Thanks John, that makes sense.

Martyn, Principal CAE Engineer, Renishaw PLC
NX12 Tc12