Cancel
Showing results for 
Search instead for 
Did you mean: 

Hole callout limitation

Phenom
Phenom

Hi,

I'm not able to add hole callout dimension to the thread in the section view. Which are the hole callaout limitiation ?

Attached part files.

Thank you...

Using NX1859
RuleDesigner PDM

13 REPLIES 13

Re: Hole callout limitation

Phenom
Phenom

If you are using “Symbolic Threads” in your model, use “Feature Parameters” command which gives a better response.

mf_201700719_01.JPG

 

 

I find “Hole Callout” has many limitations and unpredictable behaviour. (Sometimes work and sometimes not)

 

Few of my ERs (page1of4)

mf_201700719_02.JPG

 

Unpredictable behaviour:

https://www.youtube.com/watch?v=IFfY8QK2LE8

 

Check these out too.

https://www.youtube.com/watch?v=e2e9q62YMQI

https://www.youtube.com/watch?v=dOxg5tyYLBc

https://www.youtube.com/watch?v=UngJdcBCG_c

 

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Hole callout limitation

Phenom
Phenom

Hi @mike_fdo,

I use “Feature Parameters” command, but I'm a CAD reference for my collegues and I can't suggest command that are hidden and no more supported. Anyway, I confirm that Hole callout need to be implemented.

Thank you...

Using NX1859
RuleDesigner PDM

Re: Hole callout limitation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

In NX10 i'm able to place a hole callout on a symbolic thread.

 

The models needs to be fully loaded and use the quick pick to select the symbolic thread.

default NX will select first the hole feature.

 

See Movie how to select the symbolic thread.

(view in My Videos)


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Hole callout limitation

Honored Contributor
Honored Contributor

This topic came up here, as we use both methods of dimensioning threads, because there is no single method that works for everything.  When I inquired about "Feature parameters" being retired, this was the response I got from GTAC:

 

I've talked with the Developer on ER 7776177. There are currently plans to put this enhancement into a near future release. Additionally, there is currently no retirement release set for Feature Parameters. This tool will not be enhanced, but it will at least remain available for use until a retirement release is set. It seems to be almost certain that the fix for the issue will be implemented before Feature Parameters is retired, thus you should have a workaround until the issue is fixed.
-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Hole callout limitation

Phenom
Phenom

Re: Hole callout limitation

Phenom
Phenom

Hi @ruud_vandenbrand,

sorry but you have to try in the same condition before to say that the command works fine.

Thank you...

Using NX1859
RuleDesigner PDM

Re: Hole callout limitation

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Mike,

When i click the links...it says "No videos were found"

Best Regards

Kapil Sharma

Re: Hole callout limitation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Maybe YouTube took them down because they were showing both pros and cons...  Smiley Wink

Re: Hole callout limitation

Phenom
Phenom

Smiley LOL I will repost/correct the links little later. They are in editor's mode.

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW