Cancel
Showing results for 
Search instead for 
Did you mean: 

Hole diameter / size change with synchronous ?

Genius
Genius

Hi

How to change hole diameter / size with synchronous ?

  • Enlarge existing holes with some tool ?

Hole look.jpg

Hole size.jpg

4 REPLIES

Re: Hole diameter / size change with synchronous ?

Siemens Phenom Siemens Phenom
Siemens Phenom

There are two things you can try. The first thing I would do is a join face command to make it circle with one face. Then you can use resize face to change the diameter. 

 

If that does not work you can try offset region since you have 4 faces, that command does have the ability to give you the desired output.

 

Scott

Re: Hole diameter / size change with synchronous ?

Phenom
Phenom

If it is an unparametrize body, first try the optimeze faces command in synchronous modeling.

 

Ciao

Re: Hole diameter / size change with synchronous ?

Genius
Genius

How do "Move Face" and "Offset Face" differ ?

  • I confuse which is which all the time and found out something like "Offset Face" moves all faces and "Move Face" just one face. What is the reason why this happens ?

Offsetsas.png

Re: Hole diameter / size change with synchronous ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Move Face is utilized more for translating/rotating features. I cannot use offset face for this. Below are some examples.

synch_1.jpg

synch_2.jpgsynch_3.jpg

Best Regards

Kapil