Cancel
Showing results for 
Search instead for 
Did you mean: 

Hole dimension call out with tolerance in one click

Experimenter
Experimenter
Hello people,
In my work, we will use only one tolerance ie H7 for hole & g6 for shaft.Currently we are providing dimensions using 'Diametrical dimension' for the hole and 'cylindrical dimension' for the shaft respectively and then adding tolerance.I wanted to create a command such that the tolerance comes along with the diametrical dimension in a single click of a mouse.Is there a way to it? Thanks in advance
1 REPLY 1

Re: Hole dimension call out with tolerance in one click

Genius
Genius

In your drafting standards , change the Tolerance Types to Limits and Fits instead of No Tolerance

tol.PNG

and set your default tolerances in customer defaults

tol_2.PNG

 

This will however display these values even when placing horizontal or vertical dimensions...

My advice is to simply set the default fits and manually turn the tolerance on for desired dimensions... Just two clicks more.