Cancel
Showing results for 
Search instead for 
Did you mean: 

Hole series - Create solid (option:None)

Valued Contributor
Valued Contributor

Sorry if it's a repost.

 

Can anyone explain why Hole Series doesn't have an option "None" like the other Holes have, which allowes creating of solids instead of subtracting them and also if it's possible to somehow turn on that option? I can't access it through NXOpen api.

 

Thanks

 

3 REPLIES 3

Re: Hole series - Create solid (option:None)

Phenom
Phenom

Hole Series is designed to work with Assemblies.

What would you like to do with Boolean=”None”?

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Hole series - Create solid (option:None)

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @JakovM,

 

Existing enhancement request (ER) 2108180: "Boolean option for Hole Series does not contain None option".

 

As @mike_fdo questioned - what's your intent?

 

Regards, Ben

Re: Hole series - Create solid (option:None)

Valued Contributor
Valued Contributor

Thank you both for the answer and for the ER.

 

I'm aware it's meant for assemblies and that is where we use it. We use the hole series on multiple plates (mould/die design) and there are time where it's more simple (nice) to create a solid instead of a hole where that hole gets "modified" later on a part level.