Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How can I disconnect the link of component with parent?

Creator
Creator

Case 1)

I make a intersection curve using two bodies

then I want to delete the bodies (not hide)

but if I delete one of the bodies, the curve die.

 

Is there a good way to use the curve and delete bodies?

 

Case2)

I sketch a circle on A-body and make an extrude (named B-body) with the sketch.

Then

if I move A-body, the sketch also moves and B-body too.

If I want to move only A-body (not moving B-body), how can I do this easily?

 

..So I want to disconnect the link with parent component ( ex. intersection curve<->bodies , sketch <-> body )

 

Please help me with simple method.

 

Thanks a lot.

5 REPLIES

Re: How can I disconnect the link of component with parent?

Experimenter
Experimenter

Case2)

 

Sketch will always be associative to it's plane.

So instead you can use unasociative curves for your operation.

Insert > Curve > Lines and Arcs, toggle off "Associative", then select the type of curve you want to create, those will not be associative to the selected geometry/parent.

 

Thanks,

Sachin

Re: How can I disconnect the link of component with parent?

Experimenter
Experimenter

Case1)

 

After creating the intersection curves, remove parameters by selecting the section curve feature from Part Navigator.

 

Edit > Feature > Remove Parametrs.

 

 

Thanks,

Sachin

 

Re: How can I disconnect the link of component with parent?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Joooon,

Case1 - Depending upon the associativity of the derived curves needed, you can use 'Delete Body' command. 

 

Case2 - If extrude is created with no boolean operation with parent body then 'Move Object' with settings 'Move Parents - OFF' and 'Associative - ON' will give you the desired result.

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: How can I disconnect the link of component with parent?

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

In both cases I would be inclined to use non-associative Composite Curves.  This prevents you from creating dumb geometry and allows you to reconnect (reassociate) the defining geometry down the road, rather than removing parameters.

 

(view in My Videos)

 

Regards, Ben

Re: How can I disconnect the link of component with parent?

Creator
Creator

Thanks a lot!