Cancel
Showing results for 
Search instead for 
Did you mean: 

How can I set for display boundery highlights when I execute sew command and have some gaps?

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

I am NX11 user.

 

When I execute sew command and evenif there are some error like as gap or overlaps.

I cannot see a highlight a boundery for issued area.

 

How can I set for display a highlight?

 

13 REPLIES

Re: How can I set for display boundery highlights when I execute sew command and have some gaps?

Siemens Phenom Siemens Phenom
Siemens Phenom

Menu > Analysis > Examine Geometry.

Set All the checks > Examine Geometry, once check is completed there will be option 'Highlight Results' which should be toggled on to highlight/view the result in the UI.

 

Capture.JPG

 

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: How can I set for display boundery highlights when I execute sew command and have some gaps?

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Thank you for your answer!

 

But, I want to check at the same time with when I executing sew command.

 

Best regards.

Re: How can I set for display boundery highlights when I execute sew command and have some gaps?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Looks like a good ER to me ... can you  please file one for the same.

Regards

Kapil

Re: How can I set for display boundery highlights when I execute sew command and have some gaps?

Siemens Phenom Siemens Phenom
Siemens Phenom

Are you importing a IGES file in NX and using the Sew command?

 

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: How can I set for display boundery highlights when I execute sew command and have some gaps?

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Thanks to your attention for this issue.

 


I just create one block and used Unsew command for create sheet body.

 

And then I executed sew command for recreate solid body.


This issue was found by my customer, and I need to answer for this issue.

 

 

So, I'm testing and finding solution for this issue.

Re: How can I set for display boundery highlights when I execute sew command and have some gaps?

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Additionally...

 

There are no issue on my system...

 

But, appear on my customer's system...

 

 

Thank you!

Re: How can I set for display boundery highlights when I execute sew command and have some gaps?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Make sure that you have the latest MR installed. Reference this thread:

https://community.plm.automation.siemens.com/t5/NX-Design-Forum/sewing-sheets-to-solid-bodies/m-p/36...

Re: How can I set for display boundery highlights when I execute sew command and have some gaps?

Gears Phenom Gears Phenom
Gears Phenom

Simply hit the 'show result' button before to hit the 'ok' button in wireframe mode.

 

Ciao

Highlighted

Re: How can I set for display boundery highlights when I execute sew command and have some gaps?

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Assuming that your using NX11.0.0 mp1 or NX11.0.1 (which both have the fix).

 

If you hit Apply, rather than OK when using the Sew command, the gaps are highlighted.

 

Regards, Ben