Showing results for 
Search instead for 
Did you mean: 

How can i rendering cast iron or cast aluminium component in with Advanced Studio




it's possible to render a component same as the photo?

Or how can I else render a component so is just like a cast iron or aluminum component?

Firstly I give a component a material for example iron. After that I change in Studio Material Editor the type to TextureLookUp and paste a png-file. But the problem is that the rendering is not similar in every part of the cylindrical component.

What I have to set up so that the rendering is equally.


I use NX 11.


Thank You,


Component Should look like this.





My TextureLookUp-file: