Cancel
Showing results for 
Search instead for 
Did you mean: 

How edge rip works ? (rookie question)

Genius
Genius

Hi

Flat-Pattern and sheet metal creating complains about "edges to be ripped..."

-> No Flat-Pattern created therefore.

The problem corner is in [picture 1] below and it needs to be "more open"...

  • *How edge rip works ? ( I now use Modeling->Extrude and open the corner [picture 2] with raw extrude power, but is there a better method what is this edge rip ? )

Edge rip.jpg

Extrude corner Flat Rip.png

2 REPLIES 2

Re: How edge rip works ? (rookie question)

Siemens Phenom Siemens Phenom
Siemens Phenom

Edge rip is used to split a face that has no edge at all - so if the lower flange was not disconnected (at red line) edge rip could be used to create that split.

 

If you want a gap, then Normal Cutout is a better option than extrude as the edge face will be perpendicular to the sheet faces and create the correct edge for flat pattern.  One method is to unbend-cutout-rebend as shown below.

2017-01-31 13_41_42-NX 11.0.1.11 - Sheet Metal - [sheet_metal_model4.prt (Modified) ].jpg

Re: How edge rip works ? (rookie question)

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

like dave is telling is that the edge rip is use to split faces.

In this feature you can split corner edges (here you can select the edges)

for faces that needs to split you need to create curves for where the split needs to come.

 

in you use the convert to sheetmetal wizard you see at the step edge rip the options:

Select edge (existion edges)

Select section (curves)

 

in the added movie you see what this is doing.

Unable to play video. Please try again later.
(view in My Videos)


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions