Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How to Fix the object in motion for pick and place in NX MCD?

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi,

 

This is Pramod S, I am very new user of NX MCD.

 

Objective of the design: The conveyor carrying part would stop when the distance sensor's value becomes 190mm. The picking unit should slide down and attach the component, move up to its home positioin. Vertical guide along with picking unit and component should move in horizontal direction to a distance of 250mm. Picking unit should slide down and detach the component on to the different conveyor which starts with the presence of the component.

 

Problem

1. Fixing the component on the conveyor to the picking unit.

2. Sensor is disabled when I gave stick on collision condition for both the component and picking unit.

 

Help me in fixing the above issues.

Assembly Picture.PNG 

1 REPLY 1

Re: How to Fix the object in motion for pick and place in NX MCD?

Genius
Genius

Hi,

fixed joint --> object from trigger. (see the ziP file)