Cancel
Showing results for 
Search instead for 
Did you mean: 

How to acess NX 12 Topology Optimization

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi,

I am trying to swithch to topology optimization in NX. 

 

I dont see a dedicated Tab for Top opt.

 

Thanks You,

Sanjay Capture.JPG

13 REPLIES 13

Re: How to acess NX 12 Topology Optimization

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Sanjay_B,

It's a add-on. You need to download it from SPLM Download Server.

To download go to "NX > Full Products > NX12 > Windows (64-bit) > Add-Ons > Topology Optimization"

Re: How to acess NX 12 Topology Optimization

Genius
Genius

It was until NX 12.0.1 an add-on.
In NX 12.0.2 it's in the installation. Take a look into your NX 12 folder if there is already a subfolder "Topology_optimization".
When you have different NX installations maybe you need to set the path in a startscript
set NX_TOPOLOGY_OPTIZATION_DIR=%UGII_BASE_DIR%\TOPOLOGY_OPTIMIZATION
and yes: there is a Typo (not from me :-)

Re: How to acess NX 12 Topology Optimization

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi,

 

I have installed NX 12.0.2

 

I see a folder Topology Optimization.

 

How do in Integrate it/Enablle in NX UI.

 

Does it require additional download? 

 

Thankyou,

Sanjay

 

1.JPG2.JPG

Re: How to acess NX 12 Topology Optimization

Genius
Genius

There is no need for additional DL. I have in this dir ~86MB.

Do you have a license (sc_des_topol_opt)?

Then RMB for additional ribbon.

Re: How to acess NX 12 Topology Optimization

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Even the directory I have is same size.

I do have license: sc_des_topol_opt. 

RMB: Dint find Topology Optimization like yours

Check in Customize aswell 

1.JPGsize3.jpgRMB on ribbonCustomize.JPGcustomise

 

Highlighted

Re: How to acess NX 12 Topology Optimization

Siemens Genius Siemens Genius
Siemens Genius

Open or create a new .sim file and you will be able to see it.

Re: How to acess NX 12 Topology Optimization

Siemens Legend Siemens Legend
Siemens Legend

You should not have to create a new .sim file. Top Op is a designer tool and should appear in Modelling

Re: How to acess NX 12 Topology Optimization

Siemens Legend Siemens Legend
Siemens Legend

Ok so I spoke with the Product Manager for Top OP and the recommendation is that you download it from GTAC and install as per the instructions inlcuded in the download. It is a licensed product so you will need a license file with it in too.

 

Hope that helps

 

Paul

Re: How to acess NX 12 Topology Optimization

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

 

I checked the Add on its not available for 12.0.02 the version i have installed.

 

And as shown by  @Thomas_Kthis version has it pre installed, and working for him.

 

I have Raised in GTAC will update once i get a solution. 

 

 


1.JPG2.JPG