Cancel
Showing results for 
Search instead for 
Did you mean: 

How to add box around text in a note?

Genius
Genius

Is it possible to add a box/outline around some text in a note?  I have a drawing that just needs to have a box around some text.  Thanks

13 REPLIES 13

Re: How to add box around text in a note?

Phenom
Phenom

Click the GD&T box then start typing your note.

Should look like the text below.

 

<&70><+>YOUR NOTE HERE<+><&90>

Re: How to add box around text in a note?

Genius
Genius

Thanks for the fast reply!  I did try that but found that I couldn't control the size of the box unless I just changed the font size of the text.  Since you have also recommended this approach, I'll accept this as solution and quite trying to fight it.  Saved me some time!  Thanks

Re: How to add box around text in a note?

Phenom
Phenom

Have you tried changing your height factor in the settings?  You may want to play with some of these setting which may help you out a bit.

Re: How to add box around text in a note?

Genius
Genius

That's what I ended up doing and it provided a reasonable solution.  Thanks, again, for the help - I do appreciate it.

Re: How to add box around text in a note?

Phenom
Phenom

@s_hightower wrote:

Is it possible to add a box/outline around some text in a note?  I have a drawing that just needs to have a box around some text.  Thanks


Add text in 'Tabular Note'.

Thank you...

Using NX1859
RuleDesigner PDM

Re: How to add box around text in a note?

Experimenter
Experimenter

Hello, is there any possibility to define to note acoording this:

If the NOTE will overlap any model lines etc. , these model lines will be hidden and the NOTE will be visible (not crossed with other lines of model).?

Re: How to add box around text in a note?

Valued Contributor
Valued Contributor

We would need a picture.

It seems that you could do somthing on the modeling side where the box is a body feature then you could use the text feature.

  1. Make text feature
  2. Make Parametric box
  3. Make box expressions dependant to text size

On the drawing view, display the wireframe through solids

 

Cord

Re: How to add box around text in a note?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If the text is above a crosshatch, there is a way to hide the crosshatching under the text.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: How to add box around text in a note?

Experimenter
Experimenter

Can you please explain me how to do it in the case of crosshatch?

 

Thanks,

 

Lukas