Cancel
Showing results for 
Search instead for 
Did you mean: 

How to configure Reuse Library inside teamcenter to use native directories

Gears Phenom Gears Phenom
Gears Phenom

In the latest "Monthly Summary List of GTAC Technical Newsletter Articles", I saw the article:

 

How-to-configure-Reuse-Library-in-teamcenter-to-use-native-directories.docx - NX
How to configure Reuse Library inside teamcenter to use native directories

 

This intrigued me, wondering how accessing a reuse library in the native world, would work when everything else is in Teamcenter, so, I began testing.  Since we currently only have the AIA_NAS machinery library installed in Teamcenter, and we have been debating which other libraries to add.

 

Article is meant for NX10 plus, but I got it to work with NX9, even found the "ReuseLibraryConfiguration.krx" which can't be exported until NX10, and I got it working for our group, via the Customer Defaults.

ReuseLibrary.JPG

BUT, if you try to add any of this hardware, if fails.

ErrorMessage.JPG

Not surprising actually, but the article didn't mention what would, or would not work...

 

So, what types of things would work from the native world, in TC managed NX?  I have an IR in with GTAC, on this too.

-Dave
NX 11 | Teamcenter 11 | Windows 8.1
1 REPLY

Re: How to configure Reuse Library inside teamcenter to use native directories

Gears Phenom Gears Phenom
Gears Phenom

From GTAC:

Hi Dave,
I found that even though the Machinery Library will not work in managed NX from the o/s, both ‘Reusable Objects’ and ‘2D Sections’ will.
Also, you can setup so that the Drafting Symbols library can be managed on the o/s when in Managed NX from the ReUse Library tab.
Please feel free to let me know if you have any questions or concerns o this.
Best wishes,
~Angie Deering
-Dave
NX 11 | Teamcenter 11 | Windows 8.1