Cancel
Showing results for 
Search instead for 
Did you mean: 

How to create Frame design

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

 

I am quite new in NX and start to learn how to use it. and i have a question on how to create a frame design in NX. the following image is the frame design that i want to achieve. can anyone help me on how to create it? thank you very much

 

 Frame.jpgFrame design

 

6 REPLIES 6

Re: How to create Frame design

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

If you dont't have routing licenses and/or if you are not familiar with it, I would go with the Reuse Library stuff.

Create an empty assembly and add the components by drag&drop. Make sure you use the clone option in the dialog that appears after drag&drop.

See also Documentation for Knowledge Enabled Components

 

Johannes

 

reuselib.png

Re: How to create Frame design

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Johannes,

Thank you for your feedback, basically i have the license for routing, should i start the frame design from ship building? or Mechanical routing?

 

to do it with reuse library as you mentioned, can we control the the connection? ( mitter or Butt).

 

Howover thank you and i will try as your replied

 

Re: How to create Frame design

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

looks like you have a full demo license (Ship module is not common outside the shipbuilding industry).

Go with Routing Mechanical, if you'd like to use it. It has a cope (for butt connections) and also a miter option. Both is included in the "Assign corner" command.

 

Johannes

Re: How to create Frame design

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Destian,

To me it seems Steel Structures (ship building) is an overkill in your case.Offcourse you can utilize Detailed steel structure for creating these frames but you might have to customize your ship library to accomodate rectangular channel sections as well (i do not remember using any closed section profile till date but i might be wrong also).

As Johannes suggested you can through Mechanical Routing or can utilize Reuse Library for the same.

One question please ...are you creating something for the Offshore Structures???

Let us know.

Best Regards

Kapil

Re: How to create Frame design

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Jobannes,

 

Here an example using Mechanical Routing and add assign corner. the mitter connection is inactive any idea why?

Mech Route.png

 

Basically i would like to create structure for machine design (automation machine) for jig & fixture.

 

 

Please advise

Highlighted

Re: How to create Frame design

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

you also need to activate the Piping&Tubing application, then the options should be available. The Routing Mechanical application alone is not enough.

 

Johannes