Cancel
Showing results for 
Search instead for 
Did you mean: 

How to create a circular spring in NX9

Builder
Builder

Hello,

 

Any help for creating a circular spring? Enclose a photo

 

Outer diameter Spring: 3 mm

Wire diameter: 0.4 mm

Length circumference: 247 mm

 

Thanks

 

Jose C

 

3 REPLIES 3

Re: How to create a circular spring in NX9

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

you can use law curve and tube. 

 

Example part is attached. There is necessary edit some parameters.

 

Marek S.

Re: How to create a circular spring in NX9

Builder
Builder
Hello,

Thanks for your example.

have a good day

Jose C.
Highlighted

Re: How to create a circular spring in NX9

Siemens Phenom Siemens Phenom
Siemens Phenom

Also in addition to that part, NX provides examples for law curves in the reuse library samples that everyone gets.In addition to other kinds of objects. 

 

Reuse.pngSample Reuse Included with NX

 

Scott