Cancel
Showing results for 
Search instead for 
Did you mean: 

How to display a long length part in NX

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

I have NX part that has length 100m but I cannot see all of them.

It is cut at some length.

how to display all of them. 

5 REPLIES

Re: How to display a long length part in NX

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

when ever that thing happens to me. I just press "control F" or right click on background then Fit.

Re: How to display a long length part in NX

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

No it cannot solve by fit command.

I think, it should have some option to expand the range of display but I don't know where is it?

Re: How to display a long length part in NX

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Did you also try to use other keys to reset the clipping bounds like "end button" or "home button"?

Re: How to display a long length part in NX

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Yes,I did.

Anyway,I try to open the same file,same PC by TC Vis. it can open normally.

 

Thanks,

Ittipol P.

Re: How to display a long length part in NX

Siemens Legend Siemens Legend
Siemens Legend

1) This is imported data ?

2) can you snap a point somewhere on this data and verify that it is within 500 meters from the Absolute zero ?  (  Use "Menu- Information - Point")

 

If the geometry / data is way beyond 500 meters, you might need to increase the "display box",

It's in the customer defaults, so you need to change and then restart NX.
File- Utilities - Customer defaults- Gateway - visualization - View Screen - Maximum size for an objects bounding box. Set the value to something reasonable, i think it's a memory allocation thing.

 

Regards,

 Tomas