Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: How to do a solid with a 3D surface

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @lonesome-joe,

 

The Curve Rule on the selection toolbar should allow you to filter to "Single Curve":

 

Screenshot - 5_10_2018 , 9_01_41 AM.png

 

Note that I've also highlighted (in green) a handy-dandy option called "Stop at Intersection" which you might find helpful on your travels.  It stops a chain selection of curves where it intersects another curve.

 

Regards, Ben

Re: How to do a solid with a 3D surface

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

I've attached a similar result using Intersection Curves and N-sided surface rather than Combined Curve Projection and Thru Curves.  I also adopted @MarkLawry's suggestion of Extruding using Until Extended (upto the Mesh surface).

 

Regards, Ben

Highlighted

Re: How to do a solid with a 3D surface

Valued Contributor
Valued Contributor

The curve rule is one way to choose curves either connected, tangent or otherwise.

Another way is to create sketch groups in your sketches. It is also located in the curve rule. See pic below.

In your case you needed just one curve, but there are sometimes cases where you maybe need more than one curve. When you choose this sketch group rule it is saved in the feature, meaning that if you go back into the sketch and update the sketch group removing or adding curves, the steps afterward are also automatically updated and it is stable.

 

image.png