Cancel
Showing results for 
Search instead for 
Did you mean: 

How to do radius analysis in NX

Experimenter
Experimenter

Hi, 

 

On door trim assembly i want to do all surfaces which hasa radius less then 3.2mm. i know surfacic survature analysis in catia which shows all the radius less then 3.2mm for me. How do i do it in NX?

2 REPLIES 2

Re: How to do radius analysis in NX

Genius
Genius

I know only one analysis function to check the whole geometry for radius value (Concave Faces). But this function checks the concave faces only.

 

Regards André

Re: How to do radius analysis in NX

Genius
Genius

Hello

 

a very quick solution is to use the visual reporting tools included in the HD3D resource bar, see attached picture.

 

Meinolf

 

radius_check.png


Meinolf, , Leistritz Turbinentechnik GmbH


Production: NX10.0.3, TC 10.1.4

Testing:NX11 Beta