Cancel
Showing results for 
Search instead for 
Did you mean: 

How to export assembly to usb stick in Native NX ?

Genius
Genius

Hello

How to export the whole assembly to a usb stick in Native NX  ?

  • I have the assembly open now in NX 9.0 how to export it ?
  • I don't want to just copy the folder is MS file manager because the folder contains lots of other assemblies and files that I don't want to include.
  • File->Export->Part (Why only part i want to export assembly ?)
  • Save as would modify the current assembly structure and I would like it to remain the same.
9 REPLIES

Re: How to export assembly to usb stick in Native NX ?

Siemens Phenom Siemens Phenom
Siemens Phenom

You can do this via the Clone command. One the main clone page pick the assembly and set it to full, then make sure your load options are set to what you need on that tab. Now one the naming tab set the output directory to your data stick. Set the define naming rule to add suffix, the add a space " " character to the input box. See image below for the naming the rules.

 

Clone.pngClone Naming

 

Scott

Re: How to export assembly to usb stick in Native NX ?

Honored Contributor
Honored Contributor

UG Zip utility would work too.  From the "readme" file:

 

UGZIPC V1.0.5

Purpose:
  Exports components from an UG-assembly into a ZIP file

Requirements for this package:
  NX8.5
  WindowsXP/Vista,7 32Bit and 64Bit editions
  UG/Gateway
  UG/Open API Execute

Restrictions:
  - Does not support Teamcenter environment
  - Does not support filenames longer than 126 characters

Author:
  Heinrich Wiedemann
  Werkmeisterstrasse 1b
  87629 Fuessen / Germany
  Phone +49 171 5090 371  FAX +49 8362 8475
  email: hwiedemann@w-eng.de
  http://www.w-eng.de/ugzipc.htm
-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: How to export assembly to usb stick in Native NX ?

Genius
Genius

Why the suffix is needed ?

What happens if I don't select any suffix ?

Why can't parts be named like they already are ?

 

Re: How to export assembly to usb stick in Native NX ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

As an option...you can use a space as a suffix so thaat your file naming will remain intact.

There is one another option..but it is a bit lengthy ( more verstatile though) so i will not post it here as of now.

Best Regards

Kapil

Re: How to export assembly to usb stick in Native NX ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The reason you need the space is...the code INSISTS on changing the filename (just the way it was written)

Years ago, someone discovered that if you use a space, that is enough so the dialog thinks that you are changing the filename, but the code "behind" the dialog will strip off the trailing space, so the file names don't actually change.

 

Just one of those "funky" NX things...

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: How to export assembly to usb stick in Native NX ?

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

I found a simple copy assembly vb script the other day in Solution Center while looking for something else.  I just tried it and it appears to provide exactly what you're looking for.  I've attached the vb script, a basic assembly and a quick movie showing how to use it if you're interested.

 

Regards, Ben

Re: How to export assembly to usb stick in Native NX ?

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Ben,

 

Can you post this as a .zip file ?

 

I cannot download .7z files

 

Thanks

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: How to export assembly to usb stick in Native NX ?

Siemens Phenom Siemens Phenom
Siemens Phenom

@camster wrote:

Ben,

 

Can you post this as a .zip file ?

 

I cannot download .7z files

 

Thanks


Hi @joycejo,

 

Here is the link of the code from Solution Center.

Sample NX Open .NET Visual Basic program : copy assembly to target directory

 

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New

Re: How to export assembly to usb stick in Native NX ?

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @joycejo,

 

Files attached.

 

Regards, Ben