Cancel
Showing results for 
Search instead for 
Did you mean: 

How to fuse multiple parts in to one part ?

Genius
Genius

Hello

I have 5-10pcs parts/assemblies that I want to fuse in together to form a one solid model .PRT (for reference purposes) is this possible ?

4 REPLIES

Re: How to fuse multiple parts in to one part ?

Siemens Phenom Siemens Phenom
Siemens Phenom

File > Export > Part.

Use new or existing with other options as per your need.

 

You can also use WAVE, if you have a license for it.

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: How to fuse multiple parts in to one part ?

Gears Phenom Gears Phenom
Gears Phenom

Another option could be simplify assembly.  Requires an advances assembly license.

Re: How to fuse multiple parts in to one part ?

Siemens Legend Siemens Legend
Siemens Legend

You can also try to export parasolid. When you select all the bodies you need, they will all go into one parasolid file.

Just open/import the parasolid and you have everything in one part file.

 

If you really need them to be one body, you need to unite them afterwards.

There you might get the risk that they wont fuse if there is a gap between some of them.

In that case Simplify Assembly could help.

 

If you really need the data for visualisation/reference, you can also have a look into Assembly Outline. This gives a faceted representation of all the seperate components in the assembly. You dont need to open the components, but you still can see them and open the referenced parts.

 

The best choice depends on your use case.

Regards,

Gerrit Koelewijn

Re: How to fuse multiple parts in to one part ?

Genius
Genius

Hello

 

open the part in which you wants to import the other files, then in the NX menu select file / import / part.

This works not only with NX part files, you can import JT and SE files, too.

 

When importing NX parts the complete history tree will bee imported, using SE or JT files you'll get a single feature.

Also have a look on the options for getting the best result (groups, layer and CS setting)

 

With this method you can not only import solid or face bodys as when you use parasolid, you can also import for example curves from JT files.

 

 


Meinolf, , Leistritz Turbinentechnik GmbH


Production: NX10.0.3, TC 10.1.4

Testing:NX11 Beta