Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How to move ordinate dimension number/text parallel to the dimension

Pioneer
Pioneer

Hi,

 

I have an ordinate dimension and I wanted to move the dimension number/text  parallel to the dimension but it only seems to move in perpendcualr direction. I have attached a pic for reference.

 

Thanks.

 

 

12 REPLIES 12

Re: How to move ordinate dimension number/text parallel to the dimension

Siemens Genius Siemens Genius
Siemens Genius

Check your Text orientation settings - you probably need Text Aligned to Dimension Line.2017-08-09 16_00_38-NX 10.0.3.5 - Drafting.png

 

 

Re: How to move ordinate dimension number/text parallel to the dimension

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @Dag,

 

Unlinke regular Dimensions, Ordinate Dimensions cannot be positioned wherever you like.  It appears that you want your Ordinate Dimension to be positioned similar to how the regular dimension in orange is shown below:

Screenshot - 8_9_2017 , 9_21_42 AM.png

Using @JGray's suggestion of using "Text Aligned to Dimension Line", your ordinate dimension will appear as follows:

Screenshot - 8_9_2017 , 9_22_02 AM.png

There are other orientation methods for Ordinate Dimensions, none of which are going to produce the orientation and position you're looking to achieve.

 

Regards, Ben

Re: How to move ordinate dimension number/text parallel to the dimension

Pioneer
Pioneer

I see. That is too bad. I was thinking of using just the regular dimension but the dimension I am measuring is radial in a section view so it would be misleading to have just linear dimension. I guess I can get rid of one of the arrow heads from the linear dimension to imply radial dimension. Thanks for the info! 

Re: How to move ordinate dimension number/text parallel to the dimension

Pioneer
Pioneer
Thanks for the response. I tried that approach but it didn't let me put the text where I wanted. I used linear dimension as Ben suggested below and that seems to work fine. Thanks again.

Re: How to move ordinate dimension number/text parallel to the dimension

Pioneer
Pioneer
BTW how do you insert a picture into the message box? I tried pasting it but it doesn't work.

Re: How to move ordinate dimension number/text parallel to the dimension

Valued Contributor
Valued Contributor

Just hit the Photos icon - choose the file - wait till is loaded - hit the Done button...

 

Then the image should appear in the reply window and you have it in yours pictures on the server:

 

 

Esher.jpg

 

But sometimes the picture destroys text alignment

Re: How to move ordinate dimension number/text parallel to the dimension

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Unless your internet options prevent you from doing so.  Nothing happens when I click the Photos icon in Internet Explorer 11.  I have to use Firefox to embed any images.

Re: How to move ordinate dimension number/text parallel to the dimension

Gears Phenom Gears Phenom
Gears Phenom

IE.. There's a lesson in there... Man Wink

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Lenovo ThinkPad W540, Win7, 16GB. Developing in: Java | C | KF
Production: [NX8.5.3.3 MP11 64bit] Testing: [NX12.0.2 MP1]

Re: How to move ordinate dimension number/text parallel to the dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I use IE 11 and have no problems adding images:

junk.png

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled