Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How to set default decimal places in modeling(sketch)

Creator
Creator

I want to set default decimal places in modeling(sketch)

Screenshot_1.png

 

With this setting, I expected what I want.

 

But when I make a new modeling file, this preference setting is still '1'

 

And

after I change this (in drafting preferences), I can get 3 decimal places in sketch...

So I have to change everytime I make a new modeling file.

 

How can I make 3 decimal places in sketch default..?

Screenshot_3.png

 

Screenshot_2.png

 

2 REPLIES 2

Re: How to set default decimal places in modeling(sketch)

Siemens Phenom Siemens Phenom
Siemens Phenom

Re: How to set default decimal places in modeling(sketch)

Creator
Creator

If you start with modelling template (model-plain-1-mm-template.prt) normally from the directory (C:\Program Files\Siemens\NX 12.0\UGII\templates) Please copy this prt file to another directory firstly. And open this file and change the drafting settings. And copy this prt file to the original directory and replace with the original one and restart NX.

Now you will be able to write decimal two or more digits for the sketch.  

re.png

 

Ergun KESKİN, CAD/CAM/DRAFTING Application Engineer, DP Manufacturing


Production: {NX11}

Development: Testing: {NX11}