Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: How to unite two bodies that are not connected?

Gears Phenom Gears Phenom
Gears Phenom

How about doing a Unite using the geometry to subtract as the tool and choosing to keep the tool.

Then do a Subtract of the kept tool from the body that resulted from the Unite.

My simple test seemed to work OK.

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Lenovo ThinkPad W540, Win7, 16GB. Developing in: Java | C | KF
Production: [NX8.5.3.3 MP11 64bit] Testing: [NX12.0.2 MP1]

Re: How to unite two bodies that are not connected?

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

What's wrong with using Trim feature? It can be used to the same effect as Subtraction. Perhaps not in the 100% of cases, but in great many of them.