Cancel
Showing results for 
Search instead for 
Did you mean: 

I have 6 Questions in attributes

Experimenter
Experimenter

I am use NX 10.

My question in attached pictures.

A- How can I add (Account name) automatic from computer.

B- How can I minimize (projection angle symbol).

C- How to make it (3 digit).

D- How to make it automatic.

E- How to add (Part Created Date).

F- How to add (Part Modified Date).

 

Thank you

MohaDidan

4 REPLIES 4

Re: I have 6 Questions in attributes

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't think B can be done, unless you re-define the user-defined symbols used

A & E, possibly F can be done using a journal, but it has to be manually done (or run via menuscript or ?).  If you really want to dig deep into automation (I'm guessing not) perhaps a UDO or other API could be used.

 

Where is "C" coming from?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: I have 6 Questions in attributes

Experimenter
Experimenter

A- How can I add acomputer (User name) automatic to Drafting? Example: <W@$SH_USER_NAME>.

B- How can re size projection angle symbol, after calling by this code <W@$SH_SHEET_PROJECTION_ANGLE>?

C- coming from this code <WRef1*0@NX_Mass>, the result example (12.146423), How to make it (2 digit)?  like this: (12.15),

D- And how can add automatic units (Kg or Ibm) depend of part unit, to make the result (12.15 Kg) or (12.15 Ibm)?.

E- Has done by <X0.10@MyTimeStamp'3>.

F- I want to do it manually.

 

 

Thank you...

I am using NX 10.0.3.5

Re: I have 6 Questions in attributes

Genius
Genius
I have a solution for B:

(not sure about NX 10, but it should work there, too)

Insert -- symbol -- user defined...

there you could select the symbol and modify the size e.g. by modifying the scale.

Re: I have 6 Questions in attributes

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter
Hi MohaDidan,

A: There is no autotext or other technic which I know to show computer name automatially in a note.
B: This build-in proj. angle symbol cannot be resized. I draw my own symbol (I need only 3rd projection method).
C: Put this note in a tabular note. Go to cell settings, change format-type from "Text" to "Number" adjust decimal places.
D: There ist also no autotext I know to do this.