Cancel
Showing results for 
Search instead for 
Did you mean: 

I placed multiple holes in one sketch and they are assosiative ?

Genius
Genius

Hello

I placed multiple holes in one sketch and seems they are assosiative ?

- Why ? I had no measures inputted and no constraints and they still moved assosiative when I started placing the real measures ? Like I placed a measurement and suddenly all other holes moved a bit even the ones I had hand placed to a correct place.

Holes assosiative.jpg

1 REPLY

Re: I placed multiple holes in one sketch and they are assosiative ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you have auto-dimensioning turned on for sketches, NX will add dimensions to all the "hole points"

How those dimensions are defined is (to a user) arbitrary (I'm sure there are rules NX uses, but I don't know what they are).

I would edit the sketch (make it external if needed) and turn off auto-dimensionsing.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled