Cancel
Showing results for 
Search instead for 
Did you mean: 

Import .SLDPRT to NX?

Genius
Genius

I don't have access to SolidWorks. Is there any way to import a .SLDPRT file to NX?

 

Thanks!

15 REPLIES 15

Re: Import .SLDPRT to NX?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you have the right license, you can use file -> open and change the filter to sldprt.

Re: Import .SLDPRT to NX?

Phenom
Phenom

Just use Fie --> Open

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Import .SLDPRT to NX?

Genius
Genius

Hi @cowski1 @mike_fdo 

 

I only checked the menu File -> Import and never thought it can be simply in File -> Open.

 

Thank you both!

Re: Import .SLDPRT to NX?

Gears Phenom Gears Phenom
Gears Phenom

@surfactant,

 

File -> Open can work for all supported/licensed file formats including the neutral file formats like DXF, IGES and STEP.  The issue can be when using File -> Open the template part file that is used can cause different results compared to File -> Import into the current part that is open.

Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.6

Re: Import .SLDPRT to NX?

Genius
Genius

Hi @TimF   Thank you for pointing out the key difference between Import and Open!

Re: Import .SLDPRT to NX?

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello

 

Do you know which licence or feature is needed to have access on that?

 

Thank you!

Re: Import .SLDPRT to NX?

Siemens Phenom Siemens Phenom
Siemens Phenom

@WinnCh wrote:

Hello

 

Do you know which licence or feature is needed to have access on that?

 

Thank you!


@WinnCh, There is no additional/special license required to open ".sldprt",".sldasm" files.

Re: Import .SLDPRT to NX?

Creator
Creator

When I try this on any file other than an NX file, .Iges, .Step, X-T, or STL it gives this message.

 

......PLM XML Document failed to load.

 

Do you have to be using the PLM package for the import of other formats?

Re: Import .SLDPRT to NX?

Gears Phenom Gears Phenom
Gears Phenom
@mjleedle,

Try File -> Open and change the filetype. If it fails to open, find out from which version of software the .sldprt or .sldasm file came and please note that here in case Siemens employees might find that info useful. Also knowing which version of NX you're using might be helpful as well.
Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.6