Cancel
Showing results for 
Search instead for 
Did you mean: 

Import and work with STL file

Genius
Genius

Hello NX Users,

 

i wanna aks to is there any ways to work with stl file model

 

i insert file, but i cant work with it

 

i saved it in nx part file also but i cant work on it

 

have any idea for this guys!!!!!!!!!!!!!!!!!!!!!!

3 REPLIES

Re: convergent modeling- current features?

Siemens Phenom Siemens Phenom
Siemens Phenom

There's a lot of good information in the NX11 What's New:
https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_help/#uid:index_whatsnew:id1241822:xid1170373:...

Based on bevyboy's Convergent Modeling movie, I suspect you'll have to create your sketch separately and then project the sketch curves to the convergent body to use them:

https://community.plm.automation.siemens.com/t5/NX-Design-Forum/Convergent-Modelling-Technology-has-...

Regards, Ben

Re: convergent modeling- current features?

Genius
Genius

Thanks, that link is very helpful. I was just wondering if you could use convergent bodies in FEA or CAM

Re: convergent modeling- current features?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @AlexLee,

 

Not yet... Meaning in future versions FEA/CAE and CAM will be supported. If all goes well as soon as NX 11.0.1. But I cannot make you any promissed yet.

 

Kind regards,

 

Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software