Cancel
Showing results for 
Search instead for 
Did you mean: 

Import and work with STL file

Builder
Builder

Hello NX Users,

 

i wanna aks to is there any ways to work with stl file model

 

i insert file, but i cant work with it

 

i saved it in nx part file also but i cant work on it

 

have any idea for this guys!!!!!!!!!!!!!!!!!!!!!!

Warm Regards
Thomas Roman
Machine Designer
3 REPLIES 3

Re: Import and work with STL file

Builder
Builder

Actually I wanna Work with STL, edit in body

 

i cant use features like holes etc

Warm Regards
Thomas Roman
Machine Designer

Re: Import and work with STL file

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
Did you import the STL using the "Convergent" Facet Body Output Type? If you did you'll have more functionality available that just the standard NX or JT type. The following page lists functionality that is available with the Convergent body type:
https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_help/#uid:index_whatsnew:id1241822:xid1170373:...
The page lists Features and Reverse Engineering commands. The Reverse Engineering commands are what users have used in the past prior to the introduction of Convergent Modeling (Rapid Surfacing, Fit Surface, etc).
You cannot directly insert a hole into a NX, JT or Convergent facet body. You can extrude a sketch to subtract geometry from a Convergent body to create a hole.

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1872) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: Import and work with STL file

Builder
Builder
Got it @ BenBroad

Thanks for help man
Warm Regards
Thomas Roman
Machine Designer