Cancel
Showing results for 
Search instead for 
Did you mean: 

Import drawing preferences in NX9

Experimenter
Experimenter

Hi,

 

I have a problem in drawing preferences in Nx9. I create a new template. In this file I have modified Drawing preferences (lines colours, arrows...).

 

The problem is when I load this template in older files. I have the older drawing settings. How can I get template settings in older files.

 

Thank you for  your feedback.

4 REPLIES 4
Highlighted

Re: Import drawing preferences in NX9

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @jmartinez,

 

I suspect your options are going to be:

 

  • Manually edit the preferences in each existing part file, or
  • Edit your Drafting Customer Defaults and inherit these into your existing parts.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: Import drawing preferences in NX9

Experimenter
Experimenter

Hi Ben,

 

I get it! but how can I modified Drafting Customer Defaults? The idea would be modify Drafting Customer Defaults and inherit my personalized defaults. Is that posible?

 

Best regards

Re: Import drawing preferences in NX9

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @jmartinez,

Customize the available drafting standard in the customer defaults and save as with new name. After that you can use customized drafting standard settings to inherit them into the required part files. 

Drafting_Customer_Defaults.jpg

Re: Import drawing preferences in NX9

Experimenter
Experimenter

Solved!

 

Very thanks for your help.

 

Bests