10-18-2016 08:21 AM
HI All~
I try CatiaV5(catpart) import to NX10.
However, there is no density in the imported file.
What way is there?
10-18-2016 09:40 AM
Hello @djkim,
I'm not sure where this issue is caused, with the import, or the export.
But if I look at the Export options. Look at this help page about what it mapped from NX to Catia:
You'll find the following:
NX |
CATIA V5 |
---|---|
Part attributes |
Not supported. |
User attributes |
Not supported. |
As I believe the material and the density is stored in the NX attributes, I guess they are not exported to the Catia Part, and therefor not imported back into NX. And NX uses the default density as it would use for all new parts.
I hope this helps.
Kind regards,
Dennis