Cancel
Showing results for 
Search instead for 
Did you mean: 

Import pdf to sketch

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello everyone,

 

   I have a pdf of 2d skecth.How can i make into a active sketch using tha pdf and make a 3d model in nx!!! is there a way to create directly.

7 REPLIES 7

Re: Import pdf to sketch

Phenom
Phenom

Hi @karthik6,

it's not possible. You have to convert your PDF into DXF or DWG.

There are on-line site like http://www.convertfiles.com/ or use Inkscape.

Thank you..
Using NX1880 and RuleDesigner PDM

Built-in functions for converting units of measure

Re: Import pdf to sketch

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Thanks for the response @cubalibre00 Smiley Happy

Re: Import pdf to sketch

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

After saving it to dwg or dxf file whats the way to create a 3d model??

Re: Import pdf to sketch

Phenom
Phenom

File -> Import -> DXF / DWG and follow the wizard plus F1 to open help if you don't know the command.

Thank you..
Using NX1880 and RuleDesigner PDM

Built-in functions for converting units of measure

Re: Import pdf to sketch

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Thanks mate Smiley Happy

Re: Import pdf to sketch

Siemens Phenom Siemens Phenom
Siemens Phenom

As @cubalibre00 suggested, convert PDF to the DXF/DWG. Import it to the NX part and start the modeling using the imported file.

 

With Inkspace you can open a PDF file and save it as DXF which can be opened/imported in NX directly.

 

Sometimes I use Win Topo Freeware to convert content of PDF to image which can be opened in Win Topo and export it as DXF.

 

Re: Import pdf to sketch

Siemens Phenom Siemens Phenom
Siemens Phenom

In addition, once you have the 2D files in NX and have them in drafting there is a command that will convert a drawing of 2D curves to a 3D part. 

 

Scott