Cancel
Showing results for 
Search instead for 
Did you mean: 

Importing step files recipe

Experimenter
Experimenter

Hi Everyone!

I am completely new to this community, but I see that questions asked here are always very well replied, so decided I will try it out.

My problems is that I download CAD files from sources like GrabCAD and these are very often in step format. Since NX support several step formats (step203, step214 and step242), I dont now which version to chose and have to go through all of them until the part finally shows up. Is there somekind of recipe on how to do this or somewhere to find the format version?

9 REPLIES 9

Re: Importing step files recipe

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
If you open the step file with notepad you can find in the begin the step version that is used for the export.
If you find this you can use the best import for the step file.

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Importing step files recipe

Siemens Phenom Siemens Phenom
Siemens Phenom

You can refer to the following links to have clear understanding of difference between these formats.

 

http://www.datakit.com/en/step_protocols.php

 

http://www.datakit.com/en/step_ap242.php

 

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New

Re: Importing step files recipe

Experimenter
Experimenter
Thank you for a quick reply!

I tried this and the document started with the following:

ISO-10303-21

Is it the 03 part I am looking for, meaning step203?

Re: Importing step files recipe

Experimenter
Experimenter
Thank you, I will definitively have a look

Re: Importing step files recipe

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

here is a example of the step file in notepad ++

step_notepad.JPG

 

you can also see from which CAD systems the export has been done.


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Importing step files

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello everyone,

 

   whenever i try to import a step file i cannot see after importing it leaves a blank screen with no data in the part navigator what do i need to do in this case. what are the boxes that needs to be checked before exporting or importing.can anyone helpme in this?

Re: Importing step files

Phenom
Phenom

what method are you using to "import"?

 

File-> Open " *.stp"

 or

File -> Import -> STEP204 or STEP214

 or 

Windows Start -> Programs -> Seimens NX__-> "Step AP203" or "Step AP214"

 

There will be a .log file in the current folder, it includes information on number and types of entities imported and any errors.

 

Another possible problem is view scale, try ctrl+F (View Fit) to fit the view after import.

 

Re: Importing step files

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

i tried using both file--- new ----import & Windows Start -> Programs -> Seimens NX__-> Step AP203 or Step AP214 and .log file meant to be syslog file right?

Re: Importing step files

Phenom
Phenom

not syslog

There is a log file created by the translator.

 

It is usually in the folder where the the part file is created.

 

Depending how you run the translator it is named the same as the step file (ie 1234.stp -> 1234.log) or called UI.log or step214ug.log

 

if you can post an example step file with this problem I could test it.