Cancel
Showing results for 
Search instead for 
Did you mean: 

In NX8.5 modelling, Used model remained visible

Experimenter
Experimenter

Nice to meet you everyone.

I just start using NX for a week and understand some basics. However I hope you guys can help me. I finished my model  then i pressed + to "show solid bodies" and found that my extrude features which have been used for spilt model's surface are still remained. It were hided but body is still remained. I've tried to fix it by delete it and create new one, However that couldnt help. Maybe I touched some settings.

If you have any idea to fix this, Please help.

 

PS. my NX is in Japanese so my feature's name may not correct.

 

Best regards

4 REPLIES 4

Re: In NX8.5 modelling, Used model remained visible

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

It will be difficult for us to help with only this description.

Could you add some pictures of Graphics and Part Navigator? 

 

Regards, **bleep**

Re: In NX8.5 modelling, Used model remained visible

Phenom
Phenom

Do a command search for delete body.  Then use this command to delete this bodies.  You can also just remove these from your reference sets. 

Re: In NX8.5 modelling, Used model remained visible

Experimenter
Experimenter

Thank you DickBaardse

I cant provide you a graphic, only this Part Navigator is fine.

From top is my main body, Cutting part, Cutting feature and drafting from that cut edges.

Re: In NX8.5 modelling, Used model remained visible

Experimenter
Experimenter

sdeters

Thank you very much. This maybe the easiest solution for this.