Cancel
Showing results for 
Search instead for 
Did you mean: 

In Teamcenter's NX 3D mouse stops working ?

Genius
Genius

Hello

Why in In Teamcenter's NX9.0 3D mouse stops working ?

  • It works in Native NX9.0 but when I open Teamcenter's NX it stops working ?

3D Connexion SpacePilot Pro

 

3 REPLIES 3

Re: In Teamcenter's NX 3D mouse stops working ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @12131444,

 

This might well be due to other settings/variables being set when you start NX.

You should compare you NX syslog from you Native Session to the one starting NX Managed (TCIN).

 

Or post the 2 syslogs here, so we can have a look.

 

But look for 3Dconnexion and the settings in the syslog.

 

Kind regards,


Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: In Teamcenter's NX 3D mouse stops working ?

Honored Contributor
Honored Contributor

Make sure this variable is being set correctly:

 

UGII_3DCONNEXION_LIBRARY=

 

It should point to the proper 3DxNX.dll

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: In Teamcenter's NX 3D mouse stops working ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Another issue we've encountered (probably not your issue, but one never knows)...

The way we keep track of updates to (Moog customizations to) Teamcenter requires TC be run as Administrator.  But the Spaceball service is started as a "regular user".  So it is not available to NX (when started from TC).  I believe the fix is to have the TC startup script stop & restart the Spaceball service.  As it is restarted in "Administrator" mode, it is then visible to NX

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled