Cancel
Showing results for 
Search instead for 
Did you mean: 

Inferred Constraints: Disable Point Alignment

Valued Contributor
Valued Contributor

Hello,

In NX11 Sketching, I'd like to disable Vertical/Horizontal Point alignment from the automatic constraints, because it keeps constraining entities that shouldn't be aligned.

 

Is there a way to disable these two constraints, but still keep the automatic constraining for the rest of constraints?

 

Thank you.

MSV

1 REPLY 1

Re: Inferred Constraints: Disable Point Alignment

Gears Phenom Gears Phenom
Gears Phenom

Yes of course, in customer default as shown in thw attached image.

 

Ciao