Cancel
Showing results for 
Search instead for 
Did you mean: 

Insert a pdf image into a drawing

Pioneer
Pioneer

In NX 10

 

Is it possible to insert a pdf image into a drawing?  This is a 2d drawing with no related 3d model.

 

Thanks.

3 REPLIES 3

Re: Insert a pdf image into a drawing

Gears Phenom Gears Phenom
Gears Phenom

@DaveL3149,

No - convert the PDF to a raster image (JPG, TIFF or PNG) then in Drafting use Menu -> Insert -> Image to place the image onto the face of your drawing sheet.

Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.7

Re: Insert a pdf image into a drawing

Siemens Phenom Siemens Phenom
Siemens Phenom

@DaveL3149 ,

 

Even in latest NX version it is not supported. There are many ERs which ask that functionality. Some are listed below. Please contact GTAC to link your name so that you'll get notification when it's available.

 

ER# 6257682: PDF file to get inserted in drafting as DRATING VIEW

ER# 1916045: Insert a PDF in a NX drawing

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: Insert a pdf image into a drawing

Pioneer
Pioneer

Thanks.