Cancel
Showing results for 
Search instead for 
Did you mean: 

Install NX 10 in Windows 10

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Dear All, 

I setup NX 10 in windows 10 and have an issue and can't install , please see the picture

Capture.PNG

5 REPLIES 5

Re: Install NX 10 in Windows 10

PLM World Member Genius PLM World Member Genius
PLM World Member Genius

I don't believe the current build of NX 10 is certified to run on Windows 10. Check the install documentation. 

 

HTH,

Ryan

--
Ryan Gudorf
CAD/CAM Supervisor
Budde Sheet Metal Works, Inc.
Windows 7 Professional x64 SP1
Solid Edge V20
NX11.0.1
TC10.1.5 32 GB RAM, nVIDIA Quadro K4200

Re: Install NX 10 in Windows 10

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

From GTAC:

 

open Windows Explorer and navigate to the location of    

   the SPLMLicenseServer_v6.4.2_win64_setup.exe on the setup disk

 

         - Right click on SPLMLicenseServer_v6.4.2_win64_setup.exe and select ‘Properties’

 

         - Select the 'Compatibility' tab

 

         - Check the box 'Run this program in compatibility mode for:’

.

         - On the pull down menu, select 'Windows 7'

 

         - Select 'OK'

 

       - Execute SPLMLicenseServer_v6.4.2_win64_setup.exe

Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: Install NX 10 in Windows 10

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @Nguyennhotu,

 

Officially NX 10 is not supported on Windows 10, nevertheless it seems to run, but no guarantees. Not sure if you are trying to install the License server of the NX software.

 

The license server you are trying to install in Ver 6.x. This cannot be installed on Windows 8 and thus also not on Windows 10. (this is the version shipped with NX 10.0)

 

Therefor you must separately download the latest version from our website. Version 7.x and later is certified for Windows 8 (and will also work on Windows 10, although not (yet) ceritfied).

 

https://download.industrysoftware.automation.siemens.com/ Select here on the left, "Siemens PLM Licensing" --> Product updates --> Installs and here the prefered version.

 

After installing the license server, continue with the next step in your screenshot. Install NX. This runs fine for me, so it should be possible to install. You might want to manually start the setup files in the same directory are where the launch.exe is located.

 

Hope this helps.

 

Kind regards,


Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: Install NX 10 in Windows 10

Experimenter
Experimenter
Hello Mr DennisdeBrouwer,

I downloaded and installed Siemens PLM Licensing ver 7.20 but I got this error message again.
Please advise me.

Re: Install NX 10 in Windows 10

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @Khoatdecember,

 

Although this option was written for an older version, please try the following:

 

  • Open Windows Explore and navigate to the location of the 
    SPLMLicenseServer_v6.4.2_win64_setup.exe. (or 7.2 in this case)
    
       - Right click on SPLMLicenseServer_v6.4.2_win64_setup.exe and select 
         Properties.
    
       - Select the 'Compatibility' tab.
    
       - Check the box 'Run this program in compatibility mode for:'
    
       - On the pull down menu, select 'Windows 7'
    
       - Select 'OK'
    
        Execute SPLMLicenseServer_v6.4.2_win64_setup.exe and the license server
  • Reference
  • Make sure the image, SPLMLicenseServer_v6.4.2_win64_setup.exe, is local to the
    Windows 2012 R2 system. If SPLMLicenseServer_v6.4.2_win64_setup.exe is on a
    mapped drive, the desired compatibility change will not behave as expected.
Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software